Scheduled Maintenance Technical Publication app - My Email Notifications feature will undergo some optimization activities over the week; during that time users may receive false positive notifications or duplicated emails. We appreciate your patience as we strive to enhance the Aero portal experience.
Scheduled Maintenance We will be conducting scheduled maintenance on 4/19 from 10:00 PM EST to 4/20 9:00 PM EST. During this time MyAerospace applications will be temporarily unavailable. We apologize for any inconvenience this may cause.​​
×

Your browser is not supported.

For the best experience, please access this site using the latest version of the following browsers:

Close This Window

By closing this window you acknowledge that your experience on this website may be degraded.

Military Airplane
Military Airplane

When Your Mission Relies On Being Ready For Anything, You Can Rely On Us

During times of crisis, it is more important than ever to ensure your fleet is mission-ready.  Militaries around the world have increasingly been relied upon in the fight against covid-19, a very different battle to anything that may have been anticipated.  Yet many of the principles of planning remain the same.  At a time when assets may be called upon at any time, the ability to keep those assets ready to fly is of the utmost importance.

At Honeywell, we are right alongside our customers during these difficult times, and as such we have a variety of products and services all designed to keep aircraft where they need to be right now, up in the sky.  Explore and find out more about our solutions to keep you mission-ready.

Book a briefing with a member of our team to learn how Honeywell systems can help your fleet stay mission ready.

We have a vast range of drop-fit retrofits, modifications and upgrades, which mean that you can invest in modernizing your fleet, increasing efficiency and reliability during scheduled routine service intervals. Less time on the ground – more time in the air.

Transport Aircraft

Our drop-fit upgrades available for transport aircraft include:

Enhanced Ground Proximity Warning System (EGPWS) - Improves situational awareness throughout high workload missions by protecting against Controlled Flight into Terrain (CFIT)

Embedded GPS/INS Upgrade - Provides advanced performance navigation and enhanced velocity performance

Health and Usage Monitoring System (HUMS) - A sensor-based monitoring system that enables Condition-Based Maintenance (CBM) by measuring the health and performance of mission-critical components in aircraft

Traffic Awareness - Provides a greater surveillance range than ETCAS, significantly reducing the risk of collision while meeting current industry mandates for access to civilian airspace

Air Turbine Starter & Control Valve - High reliability, drop-in solution that provides more than 4,500 hours Mean Time Between Unscheduled Removals (MTBUR)

Cooling Turbine - Environmental Control System (ECS) components upgrade provides x2 times increase in cooling turbine reliability

Anti-Ice Valve - Addresses safety concerns of incumbent valve’s flow body separation occurrences

MILACAS-XR – Incorporates Change 7.1 logic and hybrid surveillance to provide a greater surveillance range than ETCAS, significantly reducing the risk of collision while meeting current industry mandates for access to civilian airspace.

EGPWS - Compact and easy to install system with low life cycle and maintenance costs. Improves situational awareness throughout high workload missions by protecting against Controlled Flight Into Terrain (CFIT).

TCAS - Significantly reduces the risk of collision in busy skies. Half the weight of previous systems and double the reliability.

Radar Altimeter System - Low probability of intercept/detection and twice the reliability of competing systems

Emergency Locator Transmitter - Portable Survival Emergency Locator Transponder which is automatically activated instantly upon immersion in water

HUMS - Condition based maintenance system that monitors the health of critical aircraft rotating components

Universal Search Light - Fully integrated dual-mode search light design protects gears, ensuring a longer life span and reduced maintenance costs for operators

Our maintenance, repair and overhaul services are designed to ensure our customers can access the products and services they need quickly and easily. We are supporting capability development in region through localization and partnerships with regional industry.  This means that our customers have the capability they need at a local level to support their fleet.  Making MRO faster, more efficient and helping to reduce downtime.

Honeywell has a range of satellite communications solutions designed to help your aircraft achieve fast, reliable and secure connections for your fleet.  Designed to provide mission critical situational awareness, our solutions enable fast and effective transmission of data for informed decision making, no matter the mission.

Our satellite communications hardware and software upgrades deliver enhanced capabilities and unparalleled global coverage across a variety of network solutions for both helicopter and fixed-wing operations.

JetWave:

Providing mission critical connectivity for Defense, JetWave satellite communication system allows users to connect to the Inmarsat Global Xpress (GX), which brings KA-band satellite coverage across the globe.  The GX network offers the most extensive global coverage for military airborne operators, including:

  • Over water
  • Over non-traditional flight paths
  • In remote areas

The system provides the warfighter with a constant command and control link.

For the unique environment the military operates within, JetWave and the Inmarsat Global Xpress network can enable a wide variety of mission-critical applications such as:

  • Real-time weather
  • Video conferencing
  • Large file transfer
  • Encryption capabilities
  • Inflight briefings
  • ISR video
  • Secure communications

JetWave is scalable and configurable for the wide variety of military platforms, with antenna options available for large and small airframes. Regardless of the airframe or its mission, JetWave can provide assured, high-speed, high-bandwidth, and secure connectivity to warfighters when and where they need it.

Aspire 200

A robust and reliable satellite communications system enabling helicopters to connect to SwiftBroadband service, which allows simultaneous voice and data connectivity.

The first solution to mitigate the issue of rotor blades interrupting and slowing communications from helicopters, Aspire 200, with the High Data Rate software upgrade, is faster than any other helicopter connectivity solution available today.

Sign up for our newsletter

To find out more about our mission-ready solutions sign up for our newsletter here, or book a briefing with a member of our team here