Attention: On Friday, March 13th from 10:00 PM EST to Saturday, March 14th, 09:00 PM EST, we will be undergoing scheduled maintenance to ensure all systems are flight ready. During this period, selected applications within the Customer Portal will experience temporary unavailability.
×

Your browser is not supported.

For the best experience, please access this site using the latest version of the following browsers:

Close This Window

By closing this window you acknowledge that your experience on this website may be degraded.

Important Reminder for Gulfstream Operators Upgraded to ASC 912 or Later

Important Reminder for Gulfstream Operators Upgraded to ASC 912 or Later

Operators Can Receive an Unrestricted Navigation Database

Gulfstream operators with ASC 912 or later can now receive unrestricted navigation and electronic charts databases. To receive an unrestricted INDS database, operators must notify Honeywell Aviation Services of the upgraded ASC

Prior to ASC 912 (currently 912-B), operators were unable to load the entire navigation database and electronic charts database due to memory limitations in the Advanced Graphics Module (AGM). As the databases became larger, the number of filtered airports began to impact more operators. This impact resulted in the need to remove airports with runway lengths of 5,000 feet or less from the navigation database and 7,000 feet or less from the electronic charts database. ASC 912 reallocated memory to enable full navigation database and chart loading. 

ASC 912-B also provides the following benefits:

  • Resolves the latency timer functionality that prevented the aircraft from meeting North Atlantic Performance-Based Communication and Surveillance data link requirements.
  • Raises the software level of the AGMs to Mod B (required for interfacing with FMS)
  • Adds several parameters to the Digital Flight Data Recorder (DFDR).
  • Adds the active/not active state of the CHECK PFD 1-2 red Crew Alerting System (CAS) message and the data required to determine magnetic or true heading selection.
  • Inhibits the NIC 3 and/or NIC 5 LAN NETWORK FAIL Central Maintenance Computer (CMC) message(s) with a new Loadable Diagnostics Information (LDI) file. These messages will no longer be reported when both are present.

ASC 912-B introduced one anomaly in the system, which caused minor discrepancies in the aircraft’s displayed position on airport charts and synthetic vision. ASC 912-C, however, will be available soon and corrects this anomaly. For release timing, please visit mygulfstream.com.

Please contact Flight Technical Services with any questions at FTS@honeywell.com.


Program Pilot David Rogers supports EPIC and NG FMS-equipped Cessna and Gulfstream aircraft for Honeywell Flight Technical Services. He can be reached via email at David.Rogers@honeywell.com.