Wi-Fi That Flies Wherever You Fly

With thousands of its products on aircraft around the world, and more than 100 years of experience providing satellite communications, mechanics, engines, cockpit technology and more to the aerospace industry, Honeywell is well-positioned to lead the aerospace industry’s Connected Aircraft evolution.

By the numbers

What kind of experience are you looking for?

90% say it's essential to experience a reliable, fast connection throughout thier flight, anywhere in the world

People expect connectivity on the ground and in the air

84% say it's important to have an experience identical to what they have at home or at the office.

What if your flight did not have inflight Wi-Fi?

6 in 10 travelers say they would be disappointed or frustrated on a plane without Wi-Fi

The Connected Aircraft

Honeywell is changing the way people communicate on and with an aircraft today and in the future — making the business of flying safer, more productive, and more entertaining. 

With the dawn of the Connected Aircraft, Honeywell continues to deliver safer, more efficient, more productive and ultimately more enjoyable travel experiences. From hardware to apps to services, Honeywell provides solutions to optimize bandwidth and reduce data and operating costs while creating the best possible experience for passengers, pilots, maintainers and operators.

Wi-Fi That Flies for any Airline

A consistent, global Wi-Fi experience

For airlines, it's simple: provide a fast internet connection onboard or risk losing faithful customers. According to a recent survey, 45 percent of customers said they would not remain loyal to their preferred airlines if they knew it didn't provide the best Wi-Fi. More than 21 percent of customers say they've made the switch already.

Honeywell's JetWave™ hardware, which connects aircraft to Inmarsat’s GX Aviation service, enables a fast and reliable in-flight internet solution strong enough to power your preferred entertainment solution with speeds up to 50mbps. Now your customers can stream their favorite television shows and your pilots can re-watch their favorite cat videos at 30,000 feet. (Kidding, of course!)

Wi-Fi That Flies for any Business

The same Wi-Fi speed above as below

Imagine flying across countries, between continents, or over oceans and remaining connected to the same Wi-Fi network. Well - spoiler alert - now you can. With JetWave, which connects aircraft to Inmarsat’s Jet ConneX service, you're always connected to a fast and consistent broadband service. 

Passengers will have the freedom to stay connected and use their mobile devices like they do on the ground and keep in touch with family and friends, work in the cloud, stream video and music, and keep work moving while traveling.

Reliable Wi-Fi for Helicopters

The unique environment of a helicopter – with the vibrations and rotor blades -- has previously made high-speed satellite systems nearly impossible. But regardless of the challenges, operators need to be connected. Honeywell’s Aspire 200 satellite communications system fills this gap, bringing new capabilities and functionalities to operators.

Aspire 200 and the high data rate (HDR) software package mitigates the impact of the rotor wash on the satellite communications signal, bringing faster speeds and higher bandwidths than competing systems. Now, regardless of the mission – VVIP transport, oil and gas, emergency medical, or others – pilots, passengers, and ground crews are constantly connected, no matter where they operate.

AW139 Helicopter Side View on Ramp

Wi-Fi That Flies for all Ages

Pilots and passengers will appreciate the affordable, global in-flight connectivity provided by AeroWave™ from BendixKing.

Crews will now have in-flight access to global weather services, voice, text, email and their favorite connected aviation apps. Plus passengers will enjoy the ability to send and receive emails, text messages, browse simple web pages, make and receive phone calls and more.

AeroWave’s low-cost connectivity service plan is based on prepaid hours of use – not the amount of data used - so there are no billing surprises. Airtime is only $40 USD per hour and, unlike other services it, works at any altitude all over the world. It’s that simple.

Don’t leave your favorite apps on the ground anymore. Find out how to get globally connected today.

Mission-Ready Communications

Reliable communications is vital to mission success for military operators. A high-bandwidth communications channel to and from the aircraft enhances safety and provides essential situational awareness for the warfighter. Honeywell’s JetWave system provides that mission-critical link. 

JetWave is built with mobility in mind to keep personnel connected in the theater throughout all stages of flight. Regardless of the airframe or its mission, JetWave provides reliable, consistent, high-speed and high-bandwidth connectivity to warfighters when and where they need it.

Wifi that flies

JetWave unlocks a wide variety of applications, including real-time weather, video conferencing, large file transfer, encryption capabilities, in-flight briefings, intelligence, surveillance and reconnaissance (ISR) video transmission and secure communications. And the system is scalable and configurable for a wide variety of military platforms, with antenna options available for large and small airframes. 

What's New With WiFiThatFlies

Follow The Conversation #WIFITHATFLIES


FIND US @HONEYWELL_AERO

Why JetWave and AeroWave?

jetwave chart

Contact Us

To learn more about connectivity and a connected aircraft, please fill out this form and someone will be in touch with you shortly.
Contact Us