Attention: On Friday, April 17th from 10:00 PM EST to Saturday, April 18th, 09:00 PM EST, we will be undergoing scheduled maintenance to ensure all systems are flight ready. During this period, selected applications within the Customer Portal will experience temporary unavailability.
×

Your browser is not supported.

For the best experience, please access this site using the latest version of the following browsers:

Close This Window

By closing this window you acknowledge that your experience on this website may be degraded.

Honeywell Reaffirms Commitment to Advance The Modernization Of The U.S. Army

Honeywell Reaffirms Commitment to Advance The Modernization Of The U.S. Army

Honeywell supports U.S. Army modernization efforts across several helicopter platforms and other programs

WASHINGTON, Oct. 10, 2022 — At the 2022 Annual Meeting of the Association of the United States Army (AUSA), Honeywell (NASDAQ: HON) reaffirmed its commitment to helping the U.S. Army modernize its armed forces. Over decades of service, Honeywell has contributed to key U.S. Army modernization programs, including upgrades to the battle-proven T55 engine for Chinook helicopters and Honeywell’s new HTS7500 turboshaft engine for the DEFIANT X®, currently a contender to win the U.S. Army’s Future Long-Range Assault Aircraft (FLRAA) competition.

“Today’s gray zone conflicts and advances in military technology by near-peer adversaries require our armed forces to rapidly modernize its capabilities and technologies across all domains of sea, air, land, space and cyber to ensure force readiness against emerging threats,” said Ricky Freeman, president, defense and space, Honeywell Aerospace. “The battlefield of the future will not be defined by who has the largest army or even the greatest firepower but rather the ability to employ advanced technologies, speed, range, scale, maneuverability and interoperability across all domains to enable the joint force to achieve overmatch against any near-peer threat.”

“Honeywell has a longstanding relationship with the U.S. Army that spans more than 50 years, and we have a strong understanding of its operational needs,” said Dave Marinick, president, engines and power systems, Honeywell Aerospace. “We are working with the U.S. military and our partners to modernize our armed forces so that their platforms remain relevant for the next generation of warfighters. Additionally, we are confident that the T55 engine, HTS7500 turboshaft, GTCP 36-150 auxiliary power units and other technology will exceed the expectations of the U.S. Army.”

 

Supporting U.S. Army modernization efforts

Honeywell is focused on supporting each of the U.S. Army’s six modernization priorities. Beyond our work on the T55 and HTS7500 engines, we are also providing the following support:

·       Honeywell’s rugged new series of inertial measurement units (IMUs) offers best-in-class accuracy along with the durability to survive high-shock environments of up to 40,000 G-force. These IMUs—which provide motion, position, and navigational sensing—can be used for a variety of defense applications by the U.S. Army, including in unmanned aerial vehicles.

·       Since the mid-1990s, Honeywell has produced and delivered more than 60,000 embedded global positioning system/inertial navigation systems (EGIs). Designed to provide maximum flexibility, the EGIs are used by the U.S. Army to meet challenging military requirements along with civil interoperability capabilities.

·       Honeywell's TALIN—which has over 20,000 units fielded—offers a proven, battle-tested, best-value technology solution for precise, reliable inertial navigation system (INS)/global positioning system (GPS) navigation, pointing and weapons stabilization.

·       Honeywell is investing in alternate position, navigation and timing offerings such as Celestial Navigation, Vision Navigation and Magnetic Navigation that can support near-term anti-access/area denial (A2AD) environments. Honeywell is ready to support the U.S. Army’s needs for navigation beyond the bounds of GPS.

·       Honeywell recently provided an update to the U.S. Army with the next-generation APN 209 Radar Altimeter, introducing state-of-the-art capabilities, reducing installation and integration changes, maximizing reuse and reducing sustainment costs.

 

The next era of U.S. Army aviation

Early this year, Lockheed Martin Sikorsky-Boeing selected a variety of Honeywell engine and power systems technology for the DEFIANT X® helicopter. This included Honeywell’s HTS7500 turboshaft engine, its GTCP 36-150 auxiliary power units (APUs) series, and its main engine generator and APU generator​ for the DEFIANT X®.

The HTS7500 is the newest, most advanced model in Honeywell’s family of military engines, which includes the iconic T55 engine that has powered the CH-47 Chinook fleet for over 60 years.

Honeywell’s APU for the DEFIANT X® is based on the existing, highly successful GTCP 36-150 APU series. The 36-150 APU series operating today delivers compressed air for main engine starting air-conditioning, anti-ice and heating systems. More than 20 proven variations modified for military and commercial aircraft are flying today.

 

An unmatched legacy of success

In late 2021, Honeywell reached a significant modernization milestone by completing the first engine to test (FETT) of the next-generation T55 engine as part of its Cooperative Research and Development Agreement (CRADA) with the U.S. Army for the next-generation T55 engine for Chinook helicopters. CRADA supports U.S. Army modernization efforts and will allow it to evaluate the capabilities of the newest rendition of Honeywell’s battle proven T55.

With 6,000 horsepower, Honeywell’s upgraded engine is projected to be 23% more powerful and consume 8% less fuel than the current T55, even in demanding operating conditions. New modifications also make the next-generation T55 easier to maintain with lower operating costs, delivering increased readiness for the warfighter.

In 2020, Honeywell won a competitive repair and overhaul contract for T55 engines already in service. In addition, Honeywell completed a new world-class engine repair and overhaul facility in Phoenix, a move that allowed the repair and overhaul work on the T55-GA-714A engine to be fulfilled in the same location as new engine production.

Please visit Honeywell at AUSA’s Annual Meeting, Booth #2603 in Hall B, to learn more about how we’re helping support the U.S. Army and its allies.

 

About Honeywell

Honeywell Aerospace products and services are found on virtually every commercial, defense and space aircraft. The Aerospace business unit builds aircraft engines, cockpit and cabin electronics, wireless connectivity systems, mechanical components and more. Its hardware and software solutions create more fuel-efficient aircraft, more direct and on-time flights and safer skies and airports. For more information, visit www.honeywell.com or follow us at @Honeywell_Aero.

Honeywell (www.honeywell.com) is a Fortune 100 technology company that delivers industry-specific solutions that include aerospace products and services, control technologies for buildings and industry, and performance materials globally. Our technologies help aircraft, buildings, manufacturing plants, supply chains and workers become more connected to make our world smarter, safer and more sustainable. For more news and information on Honeywell, please visit www.honeywell.com/newsroom.

Ahjay Rai
Global Communications Lead

Ahjay leads communications for Honeywell Aerospace across Americas, Europe, Middle East, Africa and India.