Notice: Our website address is planning on changing May 25. Existing links will redirect automatically.
×

Your browser is not supported.

For the best experience, please access this site using the latest version of the following browsers:

Close This Window

By closing this window you acknowledge that your experience on this website may be degraded.

Honeywell Achieves FAA Certification For First Flight-Critical Engine Part Built From Additive Manufacturing

Honeywell Achieves FAA Certification For First Flight-Critical Engine Part Built From Additive Manufacturing

3D-printed bearing housing paves the way for future certifications, solves critical supply chain shortages for complex engine parts

PHOENIX, August 19, 2020 - In a major technical milestone for both the aviation and additive manufacturing industries, Honeywell (NYSE: HON) has created the first certified, flight-critical engine part using additive manufacturing, commonly known as 3D printing. The part, known as the #4/5 bearing housing, is currently in production and was installed on an in-service engine. It is a major structural component in the ATF3-6 turbofan engine used on the Dassault Falcon 20G maritime patrol aircraft, which are used by the French Navy for patrol and search-and-rescue missions.

Designed by Garrett in the 1960s and certified in 1967, there are only about a dozen ATF3-6 engines still flying. This presents sourcing and supply chain challenges for operators of Dassault Falcon 20G aircraft. Additionally, the #4/5 bearing housing is a complicated part to manufacture — making it extremely costly for operators to replace due to the low quantity of orders placed. This challenge is combined with the high cost of tools needed to produce parts with traditional casting methods, where molten metal is poured into a mold and allowed to harden. With additive manufacturing, these parts can be printed much more quickly and in smaller quantities without the need for expensive tools. During this process, components are built from the bottom up, with layers of powdered metal fused on top of one another using a laser.

“Though there aren’t many in service, Honeywell is responsible for supporting and maintaining these engines. We had to find a way to address these supply chain issues and keep these aircraft flying,” said Jon Hobgood, vice president of manufacturing engineering, Honeywell Aerospace. “We were able to use our expertise in additive manufacturing to produce the qualified part much faster, reducing our lead time from approximately two years to two weeks.”

Parts such as the #4/5 bearing housing are considered “safety-critical” or “flight-critical” by regulatory bodies, meaning they must always function properly. Malfunction or failure of these parts would pose a major threat to passenger and crew safety and could cause significant damage to an aircraft. Safety-critical parts face increased scrutiny and must be approved by regulatory organizations like the Federal Aviation Administration (FAA) before they can be used on an aircraft, which makes the process from development to qualification a lengthy one.

Honeywell has been working closely with the FAA on the development and certification of multiple additive-manufactured components. These efforts have enabled the bearing housing to be the first component approved under the normal FAA delegated authority, further reducing the time for qualification.

“This is a major milestone for Honeywell because it demonstrates the maturity of our additive manufacturing operations and paves the way for us to print more certified, flight-critical parts in the future,” Hobgood added. “It also is a major win for the additive industry, as flight-critical parts face heavy scrutiny and high standards for qualification and installation on aircraft, but this shows it can be done.”

Production is currently underway for the #4/5 bearing housing, with dozens more of the bearing housing expected to be produced the end of 2020. Honeywell began its efforts in metal additive manufacturing in 2007 at its lab in Phoenix. Today, the company produces hundreds of different aircraft components with 3D printing and has expanded its industry-leading efforts to additional operations in China, Europe, India and the United States.

 About Honeywell

Honeywell Aerospace products and services are found on virtually every commercial, defense and space aircraft. The Aerospace business unit builds aircraft engines, cockpit and cabin electronics, wireless connectivity systems, mechanical components and more. Its hardware and software solutions create more fuel-efficient aircraft, more direct and on-time flights and safer skies and airports. For more information, visit www.honeywell.com or follow us at @Honeywell_Aero.

Honeywell (www.honeywell.com) is a Fortune 100 technology company that delivers industry-specific solutions that include aerospace products and services; control technologies for buildings and industry; and performance materials globally. Our technologies help aircraft, buildings, manufacturing plants, supply chains, and workers become more connected to make our world smarter, safer, and more sustainable. For more news and information on Honeywell, please visit www.honeywell.com/newsroom.

Amanda Jensen
Sr. External Communications Specialist