Notice: Our website address is planning on changing May 25. Existing links will redirect automatically.
×

Your browser is not supported.

For the best experience, please access this site using the latest version of the following browsers:

Close This Window

By closing this window you acknowledge that your experience on this website may be degraded.

Considering an Approval for RNAV (RNP) Approaches?

Considering an Approval for RNAV (RNP) Approaches?

We Can Help!

Honeywell’s RNP Consultancy service makes the process easy and straight-forward.

RNAV (RNP) approaches, also referred to as RNP AR, have been around for more than a decade, and Honeywell has been guiding operators through the approval process since their inception. In some of the most challenging environments, these approaches lend operational standardization, final approach stability beyond circling or visual approaches, and lower weather minimums. If you’ve ever thought about adding RNP AR to your operations, read on.

What Are the Benefits of RNAV (RNP)?

Approximately 400 RNAV (RNP) procedures have been published in the US to improve arrival efficiency, and NavCanada has started implementing them at many Canadian airports as well. In addition, RNAV (RNP) approaches are beginning to appear at other international locations on an as-needed basis. Some of the benefits customers are experiencing are:

  • Accessing mountainous airports like Aspen (KASE) and Eagle/Vail (KEGE), Colorado;  Bozeman, Montana (KBZN); Monterey, California (KMRY); Medford, Oregon (KMFD); and Kathmandu, Nepal (VNKT)
  • Deconflicting traffic at airports like Chicago Midway (KMDW); Gary, Indiana (KGYY); and Trenton, New Jersey (KTTN)
  • More easily accessing airports adjacent to restricted airspace like Washington Reagan (KDCA)
  • Having a stable approach to runways that cannot support a straight-in procedure like Atlanta DeKalb-Peachtree (KPDK)

RNAV (RNP) Approaches
© Jeppesen Sanderson, Inc., 1996, 2022 (Sample chart, not to be used for navigation)

How Do I Get Approval for RNAV (RNP)?

For US operators, LOA/Ops Spec C-384 is required to conduct RNAV (RNP) approaches. While the approval process requires substantial coordination with the FAA, Honeywell’s RNP Consultancy service makes the process easy and straight-forward. Honeywell consultants create the LOA application with the required documentation and manage the necessary coordination with the FAA - all while keeping the customer well-informed. The goal is to make the RNP AR LOA process painless for the customer while providing enough information so that the customer can repeat the process independently, if necessary, to add additional aircraft to the LOA/Ops Spec at a later time.

Honeywell also offers support services like navigation database validation, which is required for RNAV (RNP) operations. Since data accuracy is critical for these types of approaches, the regulatory authorities require the coded data for the approach to be validated each cycle.

Honeywell’s service is approved by the FAA and meets the requirements for data validation.

What Does It Cost?

Honeywell offers both the consulting and navigation data validation services at a competitive price. Please email Flight Technical Services at FTS@honeywell.com for the latest pricing and more information.

Note that Honeywell offers this service only to operators whose aircraft are equipped with Honeywell avionics approved for RNP AR.

This Quick Topic Video explains the details of Honeywell’s RNP Consultancy, the approval process, and benefits of RNP AR. 

 


 

Jim Johnson is Senior Manager Flight Technical Services at Honeywell and can be reached via email at James.Johnson2@Honeywell.com.