Attention: On Friday, April 17th from 10:00 PM EST to Saturday, April 18th, 09:00 PM EST, we will be undergoing scheduled maintenance to ensure all systems are flight ready. During this period, selected applications within the Customer Portal will experience temporary unavailability.
×

Your browser is not supported.

For the best experience, please access this site using the latest version of the following browsers:

Close This Window

By closing this window you acknowledge that your experience on this website may be degraded.

Revolutionizing Aviation Safety with Connectivity

Safer Skies Begin with Seamless Connectivity

While flying remains one of the safest forms of transportation, the systems keeping it that way are under mounting pressure.

Recent high-profile accidents, near misses and air traffic management (ATM) system outages underscore the growing risks of an infrastructure built on 1970s-era technology and manual processes.

Add to that the chronic staffing shortages in air traffic control (ATC) towers and operational centers, and it’s easy to see why our national airspace system is straining to meet the demands of modern aviation – and keep passengers and crews safe.

Now more than ever, aviation safety requires next-generation connectivity.

A Connected Foundation

At Honeywell, we’re not just modernizing aviation, we’re helping build a safer, smarter, more connected ecosystem.

Our innovations are driving the shift from analog, voice-based and manual processes to a digitalized, data-driven infrastructure based on real-time communication, precise tracking, dynamic routing and integrated airspace management.

“Only Honeywell is able to harness the power of connectivity across the whole ecosystem to enhance safety,” says Steve Hadden, Vice President & General Manager, Services & Connectivity at Honeywell Aerospace Technologies. “From the cockpit to the cabin to the control tower, we enable seamless communication.”

Products Redefining Connectivity and Safety

Honeywell is elevating connectivity and safety to new heights with a portfolio of products including:

Aspire: Our Aspire 350 and 400 systems use the Iridium satellite constellation to deliver reliable, pole-to-pole voice and data connectivity to business jets, helicopters and regional airlines. The system supports International Civil Aviation Association (ICAO) approved cockpit voice and safety services to improve overall safety of operations.

HCR-25 Connected Recorder: The HCR-25 is more than a digital black box, it’s a future-proof safety tool. Capturing up to 25 hours of parametric flight data, 4 channels of cockpit voice recording and con-troller-pilot datalink communications (CPDLC), it offers real-time data streaming and cloud uploads via Honeywell’s Connected Aircraft soft-ware. It also enables faster, remote access to critical flight data for stor-age or analysis.

ADS-B Out (Automatic Dependent Surveillance – Broadcast Out): Our ADS-B Out technology is reshaping how aircraft navigate increasingly crowded skies. It transmits precise position data in real time to ATC and other aircraft, enabling more accurate tracking, optimized routing and tighter separation standards for a safer airspace.

Engineering a Safer, Connected Future

Connectivity isn’t just a convenience anymore, it’s a critical enabler of today’s advanced safety technologies.

“Honeywell’s cockpit connectivity portfolio is built around highly reliable satellite systems, because when you’re talking about air traffic control or airline operations, there’s no room for dropped connections,” said Mark Goodman, Senior Director of Satcom Project Management at Honeywell.

Adds Tom Konicki, Director of Business Development at Honeywell Aerospace Technologies, “In the military, we relied on satellite connectivity for mission-critical communications. That same secure, reliable link is what we’re now bringing to commercial aviation.”

From digital black boxes to satellite-enabled cockpits, Honeywell is delivering the connectivity that safety demands – today and for the future of flight.

Commercial pilots monitoring avionics and flight controls inside aircraft cockpit during flight.
Commercial pilots monitoring avionics and flight controls inside aircraft cockpit during flight.

Let's Connect

Visit our Connectivity page to explore how Honeywell’s aviation solutions are redefining safety through connectivity.