Attention: On Friday, April 17th from 10:00 PM EST to Saturday, April 18th, 09:00 PM EST, we will be undergoing scheduled maintenance to ensure all systems are flight ready. During this period, selected applications within the Customer Portal will experience temporary unavailability.
×

Your browser is not supported.

For the best experience, please access this site using the latest version of the following browsers:

Close This Window

By closing this window you acknowledge that your experience on this website may be degraded.

3 Ways Turbogenerators Bring Efficiency to Urban Air Mobility

3 Ways Turbogenerators Bring Efficiency to Urban Air Mobility

Urban Air Mobility describes a world of drones, personal flying vehicles and on-demand air travel that is just beginning to take shape.

Urban air mobility describes a world of drones, personal flying vehicles and on-demand air travel that is just beginning to take shape. Many UAM aircraft designs incorporate multiple electric motors that can be tilted or turned off for vertical takeoff and horizontal flight. These designs aim to provide a new kind of quiet, efficient, point-to-point aviation needed to navigate the world’s cities.

Honeywell is developing power systems for these new aircraft, including a hybrid-electric turbogenerator that combines the HTS900 turbine engine with two 200-kilovolt generators. Here are three ways this technology makes UAM aircraft better than a traditional helicopter: 

Quieter  

Turbogenerator-powered aircraft designs promise to be quieter than traditional helicopters because they use multiple electric motors connected to smaller fans or propellers, rather than a single large rotor.

Safer

Most hybrid-electric urban air vehicle designs incorporate plenty of backups – they have multiple motors driving several fans, and most include on-board batteries in addition to the turbogenerator. The goal is to be able to land safely if a component fails. Traditional helicopters, meanwhile, have only one main rotor, and often only one engine.

Cleaner

The HTS900 engine is known for its low specific fuel consumption, which refers to the rate at which the engine burns fuel each hour at specific rates of thrust. Adding the two generators to the engine makes flight cleaner and more fuel efficient, with 30% to 50% fewer carbon emissions than a traditional engine. The turboshaft engine helps further minimize fuel usage with its lightweight design.

Honeywell is already a leading provider of on-board aircraft power, with systems on thousands of airliners, business jets and military and rotary aircraft worldwide. The new turbogenerator takes that flight-proven expertise and applies it to propulsion, enabling a new era of efficient and safe electric flight.

Learn more these technologies on our urban air mobility and hybrid-electric propulsion web pages.

Chris Hawley
Director of User Experience, Honeywell

Chris Hawley helps develop new technologies as part of the HUE innovation team at Honeywell Aerospace. The team designs electronic systems that are opening up new frontiers of flight, from electric air taxis to supersonic airliners.