Notice: Our website address is planning on changing May 25. Existing links will redirect automatically.
×

Your browser is not supported.

For the best experience, please access this site using the latest version of the following browsers:

Close This Window

By closing this window you acknowledge that your experience on this website may be degraded.

Honeywell Unveils JetwWave X Satcom System To Seamlessly Leverage Viasat Ka-Band Network

Honeywell Unveils JetWave X Satcom System To Seamlessly Leverage Viasat Ka-Band Network

  • JetWaveTM X is the next-generation business aviation version of the successful JetWaveTM SATCOM system designed for the aviation industry

LAS VEGAS, Oct. 17, 2023 – Honeywell (NASDAQ: HON) today unveiled JetWaveTM X, a next-generation high-speed in-flight connectivity solution optimized for the business aviation industry.

JetWave X will provide customers with unprecedented coverage and data speeds by leveraging Viasat’s Ka-band network, including its ViaSat-3 satellites and the Global Xpress (GX) satellites from its recently acquired Inmarsat business, offering the highest capacity available in the market today. JetWave X builds upon the success of Honeywell’s JetWaveTM SATCOM system by being easier to install and having greater service network flexibility, with the capability to connect to any Viasat Ka-band satellite.

In collaboration with Viasat, Honeywell has designed JetWave X to unlock significant increases in data rates for the business aviation industry, enabling access to speeds that exceed increasing passenger demands and the most data-hungry applications of the future, with typical speeds consistently greater than 30 Mbps and as high as 100 Mbps, even in the busiest flight corridors.

Designed for mobility applications, Viasat is expanding its Ka-band constellation to include eight advanced new satellites currently under construction. These will provide additional capacity that aligns well to the needs of the business aviation market, including capacity focused on the most highly trafficked routes and over the busiest hubs. Additionally, with the unique ability to dynamically steer capacity to where it’s needed, passengers are ensured consistent high speeds wherever they fly, reinforcing why a GEO-centric approach provides the best connectivity experience for business aviation.

“The demand for fast and seamless internet connectivity has been growing rapidly in the business aviation industry as the amount of in-flight data being consumed increases dramatically,” said Jason Wissink, president, Services and Connectivity, Honeywell Aerospace. “JetWave X will connect to Viasat’s current Ka-band network at entry into service, in addition to its upcoming satellites for the network, providing greater flexibility for business jet users. We will also continue to support the current generation of JetWave systems installed and operating today. Current JetWave systems will also experience a performance boost with the existing systems being able to support the higher speeds of new JX Evolution plans.”

“This is an exciting collaboration with Honeywell, resulting in a terminal solution designed specifically for business aviation customers to access advanced, high-speed solutions over Ka-band for a broad range of aircraft, from super-midsized to large cabin business jets,” said Kai Tang, head of Business Aviation, Viasat. “Over 5,000 business jets trust in Viasat to deliver fast and consistent connectivity speeds that allow videoconferencing, streaming video, corporate VPN access, and more during all phases of flight. Looking ahead, as expectations for in-flight Wi-Fi performance from flight operators and passengers soar in concert with data demand, Viasat will continue its decades-long history of advancing the gold standard of business jet connectivity with our partners.” 

In addition to accessing Viasat’s high-performing network, JetWave X also offers a number of significant benefits including ease of installation, flexible service plans and superior Honeywell support that will enable users to select the product and services that offer the best value aligned with their needs.

Honeywell’s satellite communications systems provide operators, passengers and crew with reliable, consistent connectivity throughout the world. They serve a range of needs, including in-flight connectivity for voice and data-streaming in the cockpit and the cabin, as well as fleet tracking and aircraft management.

For more information on Honeywell’s satellite communications systems, visit aerospace.honeywell.com.

 

About Honeywell

Honeywell Aerospace products and services are found on virtually every commercial, defense and space aircraft. The Aerospace business unit builds aircraft engines, cockpit and cabin electronics, wireless connectivity systems, mechanical components and more. Its hardware and software solutions create more fuel-efficient aircraft, more direct and on-time flights and safer skies and airports. For more information, visit www.honeywell.com or follow us at @Honeywell_Aero.

Honeywell (www.honeywell.com) is a technology company that delivers industry-specific solutions that include aerospace products and services; control technologies for buildings and industry; and performance materials globally. Our technologies help aircraft, buildings, manufacturing plants, supply chains and workers become more connected to make our world smarter, safer and more sustainable. For more news and information on Honeywell, please visit www.honeywell.com/newsroom.

Adam Kress
Director, External Communications