Notice: Our website address will change on May 24, and all existing links will automatically redirect; the website will be unavailable Sunday from 2:00 a.m. to 2:00 p.m. EST.
×

Your browser is not supported.

For the best experience, please access this site using the latest version of the following browsers:

Close This Window

By closing this window you acknowledge that your experience on this website may be degraded.

Structural Control and Isolation

Overview
The D-Strut describes a proprietary vibration isolation and damping technology. The first application of the D-Strut was isolating low-level vibration disturbances generated by the attitude control reaction wheels from the fine pointing requirements in the Hubble Telescope.

Later, very rigid systems were developed, which were used to replace elements of a truss. These systems provided the same static stiffness as the elements they replaced, but drastically increased the dynamic stiffness while adding as much as 50% damping.

This has been followed with multiple Space applications ranging from protecting satellites and equipment during launch to isolating delicate instruments from vibration during operation.