-
Location
-
North America
-
Latin America
-
Asia Pacific
- |
- Sales & Service Partners
- |
-
Select Shopping Cart Account
Choose the account number for your parts ordering shopping cart. Your current cart will be saved when switching accounts.
Account# Account Name City Zip/Post Code CANCELPROCEEDMy Account
-
Industries
Industries
-
Location
-
North America
-
Latin America
-
Asia Pacific
- |
- Sales & Service Partners
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
Gulfstream 450/550 Sensor Logic Changed with ASC-912C
Gulfstream 450/550 Sensor Logic Changed with ASC-912C
Changes to the Active Position Sensor Logic
David Rogers
August 3, 2021
Gulfstream 450 and 550 operators that have upgraded to ASC-912C will observe a change in the FMS sensor logic when viewing the PROGress page or the POS SENSORS pages. The change was made to make it easier for the system to go into Hybrid mode (an alignment with G-650/500/600) and once there, prevent the system from cycling back and forth between Hybrid and GPS-D as the EPU fluctuates. This will prevent instability of the Synthetic Vision System and FMS position depiction. Hybrid should be considered normal operation unless accompanied by a ‘Check GPS Position’ or ‘GPS Failed’ scratchpad message. Hybrid mode cannot be disabled independently from the IRS. Pilots attempting to ‘deselect’ hybrid (by deselecting the IRSs on the POS sensors page) will disable both Hybrid and IRS sensors for use, defeating their purpose as an immediate backup should GPS fail.
This will result in the inability of the aircraft to coast if GPS position is lost and the FMS will revert to ground based position updating.
The EPIC system looks for the sensor with the best accuracy (i.e., the lowest Estimated Position of Uncertainty (EPU)). It’s very common to see an EPU below 0.1 nm with either Hybrid or GPS as the position data source. This could result in nuisance shuffling between them since the selection tolerance is very small. To ensure the FMS position did not bounce back and forth, Honeywell incorporated logic to prevent the sensor from shuffling due to the similar EPUs. The Hybrid IRS function utilizes filtered GPS inputs to independently calculate position data producing a tightly integrated GPS/IRS position. A Hybrid filter gain was also added that is equal to that of GPS-D but will have a higher priority for sensor selection than GPS.
Why it Works Well
Honeywell published an article explaining Inertial Reference Systems in detail several years ago that can be found on the Honeywell Pilot Gateway. Hybrid IRS is often described technically as a “tightly coupled” position sensor which provides extremely accurate position calculations. Better explained, Hybrid IRS uses components in the Inertial Reference Unit to receive GPS data from the GPS receiver. “Why is this good” you ask? The idea (and benefit) of the hybrid system is that it uses both position sources, IRS and GPS, to remove error from one another. Consider IRS – it is extremely accurate in short periods of time yet accumulates drift error that compounds over several hours. GPS position is accurate in most parts of the world but does have some errors introduced due to atmospheric conditions, satellite coverage and geometry, and interference. Hybrid blends the two, using sensor-specific algorithms to filter out error in each.
Cutting Through the Noise
Prior to Hybrid technology, the FMS received a position input on power-up that was extremely accurate, but that accuracy decreased as the IRS would drift at a rate of 1-2 miles per hour. Hybrid IRSs have algorithms that use multiple Kalman Filters to target specific inaccuracies, resulting in significantly refined position, velocity and attitude performance. Measurement data are sent through a series of Kalman filters that analyze the statistical probability of errors and continuously refine the hybrid position solution. The Hybrid solution provides for better overall position accuracy from the sensors and, in the case with later systems (referred to as “High Step II”), provide more filtering that produces a RAIM like function and also extends integrity protection levels. This allows the system to “coast” using the Hybrid Inertial Position in an environment, that for many reasons, may lose GPS. This makes RNP navigation, especially approaches using low RNP, more robust to protect against GPS outages that would otherwise lead to unexpected missed approaches.
Program Pilot David Rogers supports EPIC and NG FMS-equipped Cessna and Gulfstream aircraft for Honeywell Flight Technical Services. He can be reached via email at David.Rogers@honeywell.com.
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
Your documents are ready for you. Please click here to open.
Maximum File Size
Maximum Files Exceeded
There is an issue with invoices zip file download. Please go back and try again later. Thanks!
Maximum File Size
Maximum Files Exceeded
Your orders excel is ready for download. Please click here to download.
Maximum File Size
Maximum Files Exceeded
There is an issue with orders excel file download. Please go back and try again later. Thanks!