Attention: On Friday, March 13th from 10:00 PM EST to Saturday, March 14th, 09:00 PM EST, we will be undergoing scheduled maintenance to ensure all systems are flight ready. During this period, selected applications within the Customer Portal will experience temporary unavailability.
×

Your browser is not supported.

For the best experience, please access this site using the latest version of the following browsers:

Close This Window

By closing this window you acknowledge that your experience on this website may be degraded.

Why Front Burner's Director of Aviation Chooses AeroWave

Why Front Burner's Director of Aviation Chooses AeroWave

BendixKing’s AeroWave 100 has proven itself to be an easy, reliable, and affordable solution for twins, turboprops, and light jets.

Smaller aircrafts face many challenges when it comes to in-flight connectivity. Equipment installation is complex, and the cost of data can be very expensive. In addition, smaller aircrafts have limited options for WIFI installations because of antenna restrictions, which is not an issue for high-end business jets and airlines.

Many aircrafts today are utilizing BendixKing’s AeroWave 100, including Front Burner’s PC-12. Patrick Collins, Director of Aviation for Front Burner, is responsible for the operation of the aircraft and has come to rely on AeroWave 100 for providing connectivity for him and his customers.

Corporate pilots can have crazy schedules, and Patrick is no exception. With the help of AeroWave 100 he can now remain in constant contact with his department letting them know of any unscheduled diversions or bathroom stops. Having a constant connection has allowed Patrick to quickly adjust car reservations and contact the FBO about any changes in arrival time. Patrick also recommends using the AeroWave 100 due to its affordable in-flight WIFI. With unlimited data, as low as $39.99 per hour, Patrick feels at ease knowing that his customers are receiving the best quality for less.

 

“I would recommend the system especially for the price and there’s no per megabyte charge so I don’t feel like I have to be the WIFI police when using it.”
 
“The total cost of the Aerowave 100 is what drove my decision to use the product.”
“Honestly, for the price, the AeroWave is the best system out there. It’s nice to know that the cost per hour is always fixed so I never get any unsuspected data charges”

 

“Flight plan changes don’t happen very often, but having AeroWave onboard makes it easy to contact ops to let them know if any arrival changes or deviations”