Attention: On Friday, April 17th from 10:00 PM EST to Saturday, April 18th, 09:00 PM EST, we will be undergoing scheduled maintenance to ensure all systems are flight ready. During this period, selected applications within the Customer Portal will experience temporary unavailability.
×

Your browser is not supported.

For the best experience, please access this site using the latest version of the following browsers:

Close This Window

By closing this window you acknowledge that your experience on this website may be degraded.

TFE731 Engine Still Going Strong at 50

TFE731 Engine Still Going Strong at 50

Honeywell’s history-making TFE731 turbofan engine turns 50 this summer. The TFE731-2 was certified in August 1972 and entered production a month later. Undoubtedly the TFE731 turbofan helped spur the growth of business aviation. Fast forward five decades and we’re still manufacturing the TFE731 to power aircraft like the Dassault Falcon 900, Bombardier Learjet 70/75 and Gulfstream 150.

Every time a TFE731-powered business jet takes off, it pushes the engine’s legacy to new heights. Here are some of the numbers that set the TFE731 apart:

  • 13,000 engines produced to date
  • 9,400 engines still in service
  • 108 million flight hours to date

But the engine’s impact on business aviation and Honeywell can’t be described in numbers alone. The TFE731 was the first turbofan engine designed to meet the specific needs of business aviation; most other engines of the era were adapted from existing military jet engines. As Honeywell’s first turbofan, the TFE731 launched one of our signature aerospace businesses, eventually leading to development of the groundbreaking HTF7000 engine family, which has taken the super-midsize market to a new level of performance and reliability.    

The concepts behind the original TFE731-2 engine surfaced in the late 1960s when Honeywell recognized the need for a powerful, reliable and fuel-efficient engine that could fly coast-to-coast without refueling. Our innovative engineering teams explored many options before adapting the two-spool technology from the Honeywell TSCP700 auxiliary power unit (APU), which was used on the McDonnell Douglas DC-10.

From the very beginning, the TFE731 was a model for engine innovation. It was the first geared turbofan engine with a dual-spool design that boosted fuel efficiency and enabled extended range. The engine was named “Aviation Product of the Year” by Ziff Davis Publishing in 1975.

The TFE731-2 engine produced in the early 1970s delivered 3,500 pounds of takeoff thrust with a 30-40% fuel consumption improvement to produce the transcontinental capability operators craved. The engine was also quieter than the alternatives, which enabled operators to comply with emerging noise restrictions around airports.

Learjet and Dassault were launch customers for the new engine, but they would soon be joined by other aircraft manufacturers including Cessna, Lockheed, Israel Aerospace Industries and Raytheon/Hawker Beechcraft. Further success came as the TFE731 was widely adopted in military fixed wing trainer aircraft including the CASA 101 and AIDC AT-3.  In all, the engine has received 34 aircraft type certifications and has been produced in 80 configurations.


What’s New and What’s Next

The TFE731 engine has continued to evolve and improve to meet customers’ changing needs and requirements. The engines we produce today are more powerful, with the TFE731-60 rated at 5,000 pounds of thrust at takeoff and an incremental 12% fuel efficiency improvement.

Honeywell supports the TFE731 in the aftermarket with an extensive network of OEM-certified maintenance, repair and overhaul channel partners. Most of the fleet is covered by Honeywell’s industry-leading Maintenance Service Plan (MSP)

Two years ago, we introduced the usage-based MSP incentive program that rewards TFE731 operators for using their engines in ways that reduce fuel burn and extend operating life. Honeywell uses proprietary algorithms within its predictive monitoring services to maximize engine utilization and availability, reduce maintenance costs and improve customer operations. Under the plan, operators can earn up to 10% of their monthly service plan invoice amount.


The TFE731 continues to build its reputation for proven reliability and peace-of-mind. Decades of field experience with the most prolific business jet engine translates to advances in performance such as power density, fuel-efficiency, reliability and sustainability. Honeywell is actively working on next-generation engine architectures, connected-engine and real-time diagnostics capabilities, digital logbooks, and other innovations that will drive ever-higher levels of turbine engine performance, economy and reliability.

From a sustainability perspective, Honeywell’s engines are already certified to run on up to a 50% blend of conventional and sustainable aviation fuels (SAF), enabling operators to achieve their sustainability targets and help manage the growth of aviation’s environmental footprint.

In addition, Honeywell is on the leading edge in the development of electric power-generation and distribution systems, fuel cells and electric propulsion systems that hold enormous promise for reducing the environmental impact of aviation – all building off the legacy of the TFE731 engine. 

Aerospace Technologies Marketing

We inspire innovation. We are passionate and fearless inside and outside of work. We join forces and celebrate our global team. Now you can learn a little bit more about the amazing people that make up our culture at Honeywell Aerospace Technologies.