HONEYWELL RECEIVES CERTIFICATION TO KEEP HELICOPTERS CONNECTED AND MISSION-READY FOR OPERATORS

  • Certification allows helicopter operators to increase connectivity and ease of maintenance for safer and more reliable missions
  • Honeywell’s technologies will help pilots stay connected with key ground personnel at all times


DALLAS, March 6, 2017 – Honeywell (NYSE: HON) has received Supplemental Type Certificates (STCs) — issued by a governmental agency for approval to modify an aircraft from its original design — for its connectivity and condition-based maintenance products for a variety of helicopters. The new certification enables Honeywell’s Aspire 200 satellite communications system and Honeywell Health and Usage Monitoring Systems to be used globally. These offerings will help helicopter operators around the world throughout a variety of missions, including search and rescue, oil and gas, air ambulance, and law enforcement.

“Helicopter operators need to be able to depend on their aircraft to keep them and others safe,” said Tom Neumann, vice president, Operations, BendixKing. “These Supplemental Type Certificates allow pilots to stay connected with maintenance, operations and other personnel on the ground at all times. Pilots also avoid groundings and reduce costs by using predictive maintenance diagnostics and alerts with Honeywell Health and Usage Monitoring Systems and Vibration Expert, an onboard maintenance vibration system that detects potential issues before they affect the aircraft. This is especially important when someone’s life is on the line, as is often the case in search and rescue or ambulance missions.”

The Aspire 200 system for helicopters brings broadband speeds to the cabin while reducing the impact of rotor wash on the satellite signal, which is a first for the industry. Before Aspire 200, helicopter operators experienced unreliable connectivity because the rotor blades disrupted satellite signals. The Aspire 200 system provides cabin voice and data services through Inmarsat’s SwiftBroadband satellite system and is now certified for installation on the Augusta AW139. STCs are in development for the Sikorsky S-92, AS332 Super Puma, Airbus AS350, and Sikorsky Blackhawk platforms to provide operators with consistent and reliable broadband connectivity.

Honeywell’s Health and Usage Monitoring Systems (HUMS) and Vibration Expert (VXP) have been issued certifications for multiple helicopters by the FAA, EASA and the National Civil Aviation Agency (ANAC) of Brazil, which will allow maintainers to have onboard, sensor-based monitoring systems to measure the health and performance of helicopter components. Honeywell’s VXP solutions continuously monitor aircraft vibration data to determine component issues before they fail and have one of the most proven track records among the maintenance vibration products available.

Operators using condition-based maintenance systems have experienced results such as a 4 to 5 percent increase in helicopter availability, 30 percent reduction in mission aborts, 20 percent reduction in maintenance test flights, and 5 to 10 percent reduction in scheduled maintenance costs.

Below are the helicopter platforms listed by STC:

Aspire 200 satellite communications system

  • Leonardo AW139
  • In progress:
    • Sikorsky S-92
    • AS332 Super Puma
    • Airbus AS350
    • Blackhawk

Honeywell Health and Usage Monitoring Systems

  • Sikorsky S-76C+/++
  • Leonardo AW139
  • Sikorsky Blackhawk

Honeywell VXP Health and Usage Monitoring Systems

  • Airbus EC145
  • Airbus AS350 (pending FAA approval)

Brazilian ANAC STC for Honeywell VXP Health and Usage Monitoring Systems

  • Bell 206
  • Airbus EC135
  • Airbus EC145

Honeywell technical and business experts will be available during HAI HELI-EXPO 2017 to discuss the STCs. Visit Booth #5423 for more information.

Supporting Resources

Honeywell (www.honeywell.com) is a Fortune 100 software-industrial company that delivers industry specific solutions that include aerospace and automotive products and services; control technologies for buildings, homes, and industry; and performance materials globally. Our technologies help everything from aircraft, cars, homes and buildings, manufacturing plants, supply chains, and workers become more connected to make our world smarter, safer, and more sustainable. For more news and information on Honeywell, please visit www.honeywell.com/newsroom.

Honeywell and the Honeywell logo are the exclusive properties of Honeywell, are registered with the U.S. Patent and Trademark Office, and may be registered or pending registration in other countries. All other Honeywell product names, technology names, trademarks, service marks, and logos may be registered or pending registration in the U.S. or in other countries. All other trademarks or registered trademarks are the property of their respective owners. Copyright 2017 Honeywell.

Nicole Stewart

Nicole Stewart

Senior Media Relations Manager
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
Inclusion in this directory does not imply a channel partner is authorized to maintain, repair or overhaul all Honeywell products. Contact Sales with questions.