Honeywell Opens First Authorized Warranty and Repair Station in Colombia

Honeywell (NYSE: HON) has opened its first Authorized Warranty and Repair Station in Colombia to better provide maintenance, repair and overhaul services for military forces in the region. The new facility will give Colombia’s Aeronautics Industry Corporation the capacity and resources it needs to maintain engine fuel control units and power turbine governors for the Military Forces of Colombia and other militaries and civil customers in-region, ultimately enhancing aircraft availability and readiness.

Honeywell worked closely with Colombia’s Aeronautics Industry Corporation (CIAC) and the Aeronautical Center of Maintenance from the Colombian Air Force on infrastructure and training for the new facility. With it, CIAC now has access to Honeywell-certified aircraft parts that are available in-region. This helps drastically cut down on aircraft downtime and maintenance costs for regional military aircraft, giving operators quicker and more reliable service. Aircraft that can be serviced include Bell 212, Bell 412, C90, T27, ARAVA, C95, Cheyenne, PA-42, C208, H500, Bell 206, TH67, Bell206J, C208, C90GTX, and Y12.

This is the second Authorized Warranty and Repair Station (AWARS) certified by Honeywell in Latin America, but it is the first time in Colombia that an agreement has been established between a national entity and an original equipment manufacturer for the commercialization of aeronautical services. This project is the beginning of a long-term relationship that Honeywell hopes to establish with the CIAC and with the Military Forces of Colombia to better support and reinforce the needs of the region.

Steve Brecken

Steve Brecken

Director of External Communications
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
Inclusion in this directory does not imply a channel partner is authorized to maintain, repair or overhaul all Honeywell products. Contact Sales with questions.