Honeywell Conducts Its First Pilot Survey In China To Discover Key Challenges During Flight

SINGAPORE, Feb. 17, 2016 – Honeywell (NYSE: HON) and Civil Aviation Resource Net have conducted a recent pilot survey focusing on Chinese-licensed pilots. The survey polled civil pilots and commercial flight crews on flight operations and the key challenges and requirements they face through all phases of flight to understand their prime concerns in their current operational environment.

The survey, begun in September 2015, collected firsthand flying experiences and data from more than 3,000 pilots and cockpit crew members, of whom 53 percent were first officers and 36 percent were line captains. Nearly 80 percent surveyed fly Airbus or Boeing aircraft, and more than one-third surveyed have more than 5,000 flying hours.

“This is the first time Honeywell has partnered with China’s top aviation media outlets to conduct a pilot survey that specifically focuses on the Asia Pacific regions and China,” said Brian Davis, vice president, Airlines, Asia Pacific at Honeywell Aerospace. “Pilots shared one of their biggest concerns and needs is advanced weather alert systems that provide early warning and location of a storm and its path. The use of the latest cockpit technologies such as the IntuVue 3-D weather radar can help pilots fly safer with better situational awareness.”

Weather Challenges During Departure, Cruise and Landing

It is no surprise that weather issues are among the top concerns for almost all pilots during all phases of flight, including departure, cruise and landing.

  • For 49 percent of pilots surveyed, weather hazard and wind shear are the biggest challenges for safe operation during departure, takeoff and flight.
  • More than half (53 percent) surveyed said identifying hazardous, turbulent weather is the biggest concern in cruise flight.
  • During landing, 65 percent of respondents consider hazardous weather identification as the biggest challenge.

The use of weather radar can efficiently reduce the risk of weather issues and related delays. In this survey, 60 percent surveyed selected predictive weather alerts for lightning, hail and long-range turbulence as the most important feature of a weather radar, followed by automatic in-route weather notifications when weather radar is deactivated and continuous 3-D weather scanning and depiction.

Fly Safer With Better View and Awareness

For a better understanding of the challenges current civil pilots face, Honeywell Aerospace kept the needs of the end users in mind while conducting the survey. As the global leader in the aviation industry, Honeywell Aerospace creates some of the most cutting-edge products and technologies addressing the biggest concerns pilots face in weather detection and precision approaches.

For helping pilots make the right decisions faster in all flight phases, Honeywell’s IntuVue RDR-4000 3-D Weather Radar provides pilots with real-time and accurate weather information. As the only automatic radar system, IntuVue produces a 3-D, 180-degree image of weather from the ground up to 60,000 feet and up to 320 nautical miles (nm) ahead of the aircraft. IntuVue can even predict what storms have hail and lightning five to 10 minutes before the lightning occurs with 93 percent accuracy, which addresses the concerns of 60 percent of those surveyed. IntuVue also provides the industry’s longest turbulence detection, out to 60nm, to reduce turbulence-related incidents by more than 45 percent. This makes a great solution for over half (53 percent) of the respondents who find hazardous and turbulent weather identification the biggest challenge during flight.

Honeywell’s enhanced ground proximity warning system (EGPWS) serves as an independent monitor of an aircraft's position relative to surrounding terrain, providing airplanes with worldwide protection against controlled flight into terrain, wind shear and optional runway incursions and overruns. Its software upgrades, Honeywell’s SmartRunway® and SmartLanding® products, can increase flight safety by improving situational awareness for pilots and crew members during approach, landing, taxi and take-off.

“The aviation industry has made a continuous effort to improve flight safety all these years. It is critical for us to understand end users’ top needs and to help them address their concerns with the right solutions,” said Davis. “With our long history and long-term commitment in the Asia Pacific region’s aviation industry, Honeywell values the collaboration with domestic enterprises in the aviation industry and looks forward to working with other companies in the field for building a booming aviation industry in Asia Pacific together.”

Supporting Resources

Honeywell Aerospace products and services are found on virtually every commercial, defense and space aircraft, and its turbochargers are used by nearly every automaker and truck manufacturer around the world. The Aerospace business unit develops innovative solutions for more fuel-efficient automobiles and airplanes, more direct and on-time flights, safer flying and runway traffic, along with aircraft engines, cockpit and cabin electronics, wireless connectivity services, logistics, and more. The business delivers safer, faster, and more efficient and comfortable transportation-related experiences worldwide. For more information, visit www.honeywell.com or follow us at @Honeywell_Aero and @Honeywell_Turbo.

Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. For more news and information on Honeywell, please visit www.honeywellnow.com.

Honeywell and the Honeywell logo are the exclusive properties of Honeywell, are registered with the U.S. Patent and Trademark Office, and may be registered or pending registration in other countries. All other Honeywell product names, technology names, trademarks, service marks, and logos may be registered or pending registration in the U.S. or in other countries. All other trademarks or registered trademarks are the property of their respective owners. Copyright 2016 Honeywell.

# # #

Amy

Amy Xu

External Communications Manager
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
Inclusion in this directory does not imply a channel partner is authorized to maintain, repair or overhaul all Honeywell products. Contact Sales with questions.