Honeywell and Air India to Establish New Levels of Landing and Runway Safety


Honeywell and Air India to Establish New Levels of Landing and Runway Safety

Honeywell’s SmartRunway/SmartLanding upgrade improves situational awareness; delivers safer landing and taxiing operations

Honeywell Aerospace (NYSE: HON) has signed a Memorandum of Understanding with Air India enabling the airline to explore how Honeywell’s SmartRunway/SmartLanding software upgrade can help it increase safety, improve pilot situational awareness and lower cockpit workload across its Boeing 777 fleet. The SmartRunway/SmartLanding upgrade helps mitigate runway accidents that cost the worldwide aviation industry U.S. $1 billion annually for injuries, damage, repairs and inspections.*

"At Air India we are constantly looking for innovative ways to bring our passengers new levels of safety and comfort when they fly with us," said A. K Mathew, executive director of engineering, Air India.

"As we expand our network, our pilots are required to fly into an evergrowing number of airports, many of which are continually changing in terms of layout. SmartRunway/SmartLanding could make it easier for our pilots to navigate these airports regardless of visibility, and extend passenger safety even further in the process."

Honeywell’s SmartRunway/SmartLanding system uses GPS location information and airport and object data stored in Honeywell’s Enhanced Ground Proximity Warning System (EGPWS) database to determine if the aircraft is configured properly for landing, taxiing and takeoff. This can dramatically reduce runway incursions, where collisions occur on the runway, or runway excursions, where aircraft accidentally leave the runway or enter a runway they are not approved for.

Under the terms of the agreement, Air India will trial SmartRunway/SmartLanding for six months and share operational data with Honeywell to enable the two companies to examine the potential safety gains the airline would see if it deployed the software across its entire EGPWS-equipped B777 fleet. The software upgrade reduces crew workload as pilots spend less time orienting themselves, even in low visibility or at night. This is especially crucial as airlines grow their networks, train new pilots, ramp up traffic, and begin flying to new or rapidly developing airports.

Nearly 2,500 aircraft in service today already use Honeywell SmartRunway and SmartLanding systems (including those using Honeywell’s Runway Awareness and Advisory System (RAAS) on which SmartRunway is based) to help reduce the risk of runway and landing incidents by monitoring for more than 20 potential hazards. SmartLanding, which is primarily concerned with mitigating runway excursions, monitors for potentially unstable approaches, including if the aircraft is flying too high, too fast or has incorrect flap settings, and helps prevent long landings and accidental taxiway landings. SmartRunway mitigates runway incursions. It informs pilots which runway they are entering, confirms runway length, monitors for insufficient length remaining and can also perform flap checks to ensure proper aircraft configuration prior to takeoff. Both support "heads-up" and "quiet cockpit" through aural and visual warnings.

"Air India is looking for new ways to maximize the safety of its passengers by taking advantage of the safety systems its fleet already has in place," said Pritam Bhavnani, president, Honeywell Aerospace India.

"Because SmartRunway/SmartLanding is a software upgrade, airlines can cost-effectively add new functionality to their EGPWS with no additional weight and minimal aircraft downtime, and in doing so make operations safer -- even at new, unfamiliar airports and in low visibility."

Both SmartRunway and SmartLanding are available for commercial and business aviation platforms currently equipped with Honeywell’s EGPWS. Honeywell will be showcasing a range of its technologies at India Aviation 2014 in Hyderabad, March 12–15, at stand 19 in Hall A.

Editor’s note
*figure based on Honeywell estimates

Supporting Resources


About Honeywell India
Honeywell is a Fortune 100 company ( that develops and manufactures technologies to address some of the world’s toughest challenges linked to global macrotrends such as energy efficiency, clean energy generation, safety and security, globalization and customer productivity. Each of the company’s four businesses — Aerospace, Automation and Control Solutions, Performance Materials and Technologies, and Transportation Systems — has a significant presence in India. Honeywell’s India commitment is evident in five state-of-the-art manufacturing and engineering operations for its automation, turbocharger, and refining businesses, and five global centres of excellence for technology development and innovation. Honeywell employs more than 13,000 people across 50 locations including Delhi, Pune, Bengaluru, Hyderabad, Chennai, Gurugram and Madurai. For more news and information on Honeywell, please visit

About Honeywell Aerospace
Thousands of Honeywell Aerospace products and services are found on virtually every commercial, defense and space aircraft worldwide. The Aerospace business unit develops and integrates technologies that span air traffic modernization, flight and runway safety, engines, cockpit and cabin electronics, connectivity, logistics and more that deliver safe, efficient, productive and comfortable transportation-related experiences. For more information, visit or follow us at @honeywell_aero on Twitter.
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
To contact support, visit Please note, for the best experience, you may be asked to log in.

Search Directory

Inclusion in this directory does not imply a channel partner is authorized to maintain, repair or overhaul all Honeywell products. Contact Sales with questions.