Leading Mexico carrier signs MoU with Honeywell and Safran to evaluate EGTS electric taxiing system performance at high altitude airports
Honeywell (NYSE: HON) and Safran (NYSE Euronext Paris: SAF) have signed a Memorandum of Understanding with Mexican airline Interjet, to support the advancement of the EGTS™ Taxiing System, a technology for use on the taxiway and runway, which brings both fuel savings and emissions reductions to airlines. Interjet is the first airline in America to collaborate on the EGTS program, following easyJet, Air France and GoAir.
EGTS, the result of a joint venture between Honeywell and Safran, uses motors on the aircraft’s main landing gear to enable it to push back from the gate and taxi using its own electrical power rather than its main engines. This can save airlines as much as four percent block fuel consumption every flight. In January 2014 EGTS International announced an MoU with Airbus to explore the potential for integrating the EGTS taxiing system on the airframer’s A320 Family, under a program Airbus calls “eTaxi”.
“We have been working for a number of years with both Safran and Honeywell on innovative projects to reduce our environmental impact,” said José Luis Garcia, CEO of Interjet.
“This agreement is the next logical step in our collaboration to further reduce our carbon footprint.”
Under the agreement, Interjet will share data on its taxiing procedures and in particular, in high altitude airports, where Interjet frequently operates. The low air density prevalent in these types of airports impacts aircraft performance, requiring airlines to adapt operating procedures to these conditions. Interjet and the EGTS team will evaluate together the operational parameters required for electric taxiing operations in these environments.
“Interjet will help us to confirm that EGTS is the only on-board system currently in development capable of generating enough traction during taxiing in all weather conditions and at all airports,” said Brian Wenig, vice president EGTS Program, Honeywell.
“The partnership will also help us refine system capabilities for operation in different environmental conditions that change the demand placed on the Auxiliary Power Unit, used to provide power the EGTS motors.”
This agreement is the second environmental collaboration between the three parties. In 2011, Both Safran and Honeywell supported Interjet in its first commercial flight with biofuels. Powered by CFM56* engines, the Airbus A320 used a blend of 27 percent biofuel derived from the jatropha crop and 73 percent ordinary kerosene. The jatropha used by Interjet was grown in the Chiapas region of Mexico and converted into jet fuel by Honeywell UOP.
“We are extremely pleased to embark Interjet on this ambitious program,” said Olivier Savin, vice president EGTS Program, Safran.
“The airline has been a true pioneer in commercial aviation in Mexico since the 1930s. Supporting EGTS demonstrates once again its commitment to innovation and greener technologies for the Mexican aerospace industry.”
* CFM56 is a trademark of CFM International, a 50/50 joint company between Snecma (Safran) and GE.
Supporting Resources
- Learn more about EGTS International
- Follow @green_taxiing on Twitter
- Learn more about Interjet
Editors Notes:
Developed by EGTS International, a joint venture between Honeywell and Safran, EGTS uses electric motors on the main landing gear to enable the aircraft to push back autonomously and taxi without using its main engines.
Honeywell and Safran estimate that total savings for airlines using EGTS could range from between US$200,000 to US$450,000 per aircraft, per year, depending on their operations profile and system utilization. Allows aircraft to push back without a tug and then taxi between gate and runway without engaging the main engines by using the Auxiliary Power Unit (APU) generator to power electric motors in the main landing gear.
In addition to reduced fuel burn, the system will also generate further savings by minimizing the risk of damage to engine turbines from foreign objects on the tarmac.
The pilot maintains full control of the aircraft’s speed with virtually no use of the brake through an integrated Pilot Interface Unit. The system design offers a fast installation time and does not affect brake cooling or tire speeds on landing.
About Honeywell AerospaceThousands of Honeywell Aerospace products and services are found on virtually every commercial, defense and space aircraft worldwide. The Aerospace business unit develops and integrates technologies that span air traffic modernization, flight and runway safety, engines, cockpit and cabin electronics, connectivity, logistics and more that deliver safe, efficient, productive and comfortable transportation-related experiences. For more information, visit http://aerospace.honeywell.com or follow us at @honeywell_aero on Twitter.
Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.
About Safran
Safran is a leading international high-technology group with three core businesses: Aerospace (propulsion and equipment), Defence and Security. Operating worldwide, the Group has 66,200 employees and generated sales of 14.7 billion euros in 2013. Working alone or in partnership, Safran holds world or European leadership positions in its core markets. The Group invests heavily in Research & Development to meet the requirements of changing markets, including expenditures of 1.8 billion Euros in 2013. Safran is listed on NYSE Euronext Paris and is part of the CAC40 index. For more information, www.safran-group.com / Follow @SAFRAN on Twitter
About Interjet
Interjet, a 100% Mexican airline, is owned and operated by the Aleman family. Interjet began operations on December 5th 2005, with a fleet of three Airbus A320 aircraft, connecting three destinations in Mexico and today it has 42 A320 and 5 Superjet 100 aircraft. In December 2013, Interjet celebrated its eighth anniversary, fulfilling its pledge of quality service at an affordable price. Beginning a strong relationship with its neighboring country to the north, Interjet began operations in United States on December 1st 2011, with its first flight to San Antonio, Texas from Mexico City International Airport and on December 6th from the Toluca International Airport. Interjet has 43 routes, 34 in Mexico City and 9 international destinations : San Antonio, Las Vegas, Orange County (L.A), Miami, Nueva York, Costa Rica, Guatemala, La Habana and Bogotá. Interjet’s network also offers excellent connections to other destinations at the airport in Mexico City. For further information and reservations, consult www.interjet.com or call 866-285-9525.
Honeywell and the Honeywell logo are the exclusive properties of Honeywell, are registered with the U.S. Patent and Trademark Office, and may be registered or pending registration in other countries. All other Honeywell product names, technology names, trademarks, service marks, and logos may be registered or pending registration in the U.S. or in other countries. All other trademarks or registered trademarks are the property of their respective owners. Copyright 2013 Honeywell. This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current economic and industry conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.